I tried setting the Switch banks to boot from NAND flash. When I reset the board nothing happended.
Is there a procedure to switch the boot from NOR to NAND and do I have to install software (U-boot etc.) in the NAND flash before switching from NOR to NAND?
Thanks,
C-
Our SDK Linux for the B4860QDS board does not support booting from NAND Flash. It generates u-boot for booting from NOR Flash only.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We need to have a file system in Linux (64-bit) that supports more than 30 Mb. The NAND flash supports 512 Mb. How does one boot a configuration that allows linux to have a bigger root file system?
Change u-boot configuration file for NAND Flash on your board. See attachment. It is b4860qds u-boot configuration file.
U-boot configuration file is located in the u-boot source folder: /include/configs. This folder contains the .h files for the different boards.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Did you include the attachment you mentioned above? Is the procedure for switching to NAND also included?
Thanks,
C