i.MX6UL PHY management interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL PHY management interface

Jump to solution
1,134 Views
ko-hey
Senior Contributor II

Hi all

I have a question about "MDIO frame field".

I know i.MX6UL PHY management interface follows the standard MDIO specification(IEEE 802.3 Clause 22) and i.MX6UL has only following opcode type of operation.

Opcode defines type of operation. Programmed with ENETn_MMFR[OP].
01 Write operation
10 Read operation

From the RM, I understand "00" and "11" have never defined.
On the other hand, some Ethernet IC has "00" opcode type of operation.

Can I use "00" and "11" settings in i.MX6UL ? Please tell me both of the answer and reason.

Did NXP test the "00" and "11" setting in i.MX6UL ?


Ko-hey

Labels (2)
0 Kudos
1 Solution
923 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

according to MDIO specification IEEE 802.3 Clause 22 defines only

01 Write operation
10 Read operation

http://www.ieee802.org/3/efm/public/sep01/turner_1_0901.pdf 

http://www.ieee802.org/3/efm/public/nov02/oam/pannell_oam_1_1102.pdf 

IEEE 802.3 Clause 45 uses also "00" and "11" settings, as

described in sect.22.6.17.2 MDIO clause 45 frame format

i.MX6UL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
924 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

according to MDIO specification IEEE 802.3 Clause 22 defines only

01 Write operation
10 Read operation

http://www.ieee802.org/3/efm/public/sep01/turner_1_0901.pdf 

http://www.ieee802.org/3/efm/public/nov02/oam/pannell_oam_1_1102.pdf 

IEEE 802.3 Clause 45 uses also "00" and "11" settings, as

described in sect.22.6.17.2 MDIO clause 45 frame format

i.MX6UL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
923 Views
ko-hey
Senior Contributor II

Hi Igor

I know the specification defines only "01" and "10".

From you answer, NXP have never tested the settings of "00" and "11".

Is my guess correct ?

Ko-hey

923 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes correct.

Best regards
igor

0 Kudos
923 Views
ko-hey
Senior Contributor II

Thanks!

ko-hey

0 Kudos