AnsweredAssumed Answered

Error: max_leb_cnt too low

Question asked by Chandra Mills on Aug 29, 2016
Latest reply on Sep 8, 2016 by Yiping Wang

NOTE: Executing mklibs_optimize_image ...
DEBUG: Executing shell function mklibs_optimize_image
DEBUG: Shell function mklibs_optimize_image finished
NOTE: The image creation groups are: [['tar', 'ext2', 'jffs2', 'ubi']]
NOTE: Running image creation script for tar: /opt/QorIQ-SDK-V1.8-20150619-yocto/build_b4860qds-64b_release/tmp/work/b4860qds_64b-fsl-linux/fsl-image-flash/1.0-r0/temp/create_image.tar ...
NOTE: Running image creation script for ext2: /opt/QorIQ-SDK-V1.8-20150619-yocto/build_b4860qds-64b_release/tmp/work/b4860qds_64b-fsl-linux/fsl-image-flash/1.0-r0/temp/create_image.ext2 ...
NOTE: Running image creation script for jffs2: /opt/QorIQ-SDK-V1.8-20150619-yocto/build_b4860qds-64b_release/tmp/work/b4860qds_64b-fsl-linux/fsl-image-flash/1.0-r0/temp/create_image.jffs2 ...
NOTE: Running image creation script for ubi: /opt/QorIQ-SDK-V1.8-20150619-yocto/build_b4860qds-64b_release/tmp/work/b4860qds_64b-fsl-linux/fsl-image-flash/1.0-r0/temp/create_image.ubi ...
ERROR: Error: The image creation script '/opt/QorIQ-SDK-V1.8-20150619-yocto/build_b4860qds-64b_release/tmp/work/b4860qds_64b-fsl-linux/fsl-image-flash/1.0-r0/temp/create_image.ubi' returned 255:
Error: max_leb_cnt too low (53183 needed)
WARNING: exit code 255 from a shell command.

DEBUG: Python function do_rootfs finished
ERROR: Function failed: do_rootfs

Outcomes