Hello,
I have a problem when compiling assembler files using mwasmeppc.exe, this is the error message:
* Compiling s -> o
*
### mwasmeppc.exe Assembler:
# File: ..\output\obj\cstartup.s
# ---------------------------------
# 88: e_and2i. r3,0xFFF@l
# Error: ^^^^^^^^
# Instruction not legal for current target processor(s)
### mwasmeppc.exe Assembler:
# 99: sub r4,r3
# Error: ^^^^^
# Not enough arguments for simplified mnemonic sub
### mwasmeppc.exe Assembler:
# 114: e_or2i r31,0x4002
# Error: ^^^^^^
# Instruction not legal for current target processor(s)
Some commands( e_and2i. sub e_or2i) can not be recognized, but this file cstartup.s works with other compiler(Greenhills, Windriver, etc)
CodeWarrior version: for MPC55xxMPC56xx v2.10.
MCU: XPC560XB
the cpu type is -proc Zen
I don't know if I miss some compiler options, or I need to include some compiler files?
Best regards,
Sijia
Hi,
I have already answered your question in this thread:
https://community.nxp.com/thread/433463
Regards,
Martin