Hi,
We are using LPCXpresso54114 board along with MAO shiled(Add-on-board) for our speech recognition project.
We wanted to know overall power consumption the mentioned board including add-on-board for our design power estimation ?
Also planning to use microphone array(multiple microphone) on board with beam forming concept.
Does the LPCXpresso54114 evaluation board support beam pattern of microphone output ?
If you have any data regarding beam forming microphone array please share to us
We appreciate your quick response and thanks in advance
Hi,
Unfortunately we cannot provide a comprehensive answer because the power consumption depends completely of your application.
The LPCXpresso54114 has built-in power measurement circuitry, controlled by its onboard Link2 debug probe. This circuitry can measure power consumed by the LPC54114 by sampling the voltage dropped across a sense resistor on the board using a differential amplifier, sampled at up to 200 kHz by a 12-bit ADC. The power consumed by the MAO Shield can be measured as well, since the Shield has a similar differential amplifier/sense resistor circuit. An analog multiplexer is used to select between these measurement sources.
For more information please check the user guide http://www.nxp.com/documents/user_manual/UM10973.pdf
Regarding multiple microphone, unfortunately this was not implemented nor tested in the LPCXpresso54114 evaluation board.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------