编译器 :IAR for arm 7.50
调试器 :lpc-link2
j-link 版本:v6.00
板子是我们自己做的lpc4370的板子
工程使用的是:lpcopen_2_04_keil_iar_nxp_lpclink2_4370
进入调试的时候连接不上板子,出现:
This script is designed for working with only a LPC4350 in the JTAG chain.
确认板子的jtag和调试器链接没有问题。调试器我用LPC4330_Xplorer链接没用问题,请教一下哪里出了问题,初次使用lpc4370.
Hi,
LPC-Link2是支持各个LPC系列的MCU,除了LPC2xxx (ARM7) , LPC3xxx (ARM9).
我建议你可以按照这个帖子的方法,更新完固件后,重新调试。
【经验分享】LPC-LINK2 仿真接口使用注意事项 - ARM Cortex-M系列产品 - 恩智浦技术社区 - 手机版 - Powered by Discuz!
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------