Hi Andrew,
In addition, can you check if the objects definition files are included in the build?
in classic CW
in CW eclipse
if the problem still can not be solved, can you please upload your project here?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Link Error : L1822: Symbol TIMESEQ in file C:\Users\DE\Documents\Project_2\Project_2_Data\Standard\ObjectCode\main.asm.o is undefined
Link Error : L1822: Symbol INITSEQ in file C:\Users\DE\Documents\Project_2\Project_2_Data\Standard\ObjectCode\EXESEQ.asm.o is undefined
Link Error : Link failed
Your zip folder includes some sources files but doesn't include project file (.mcp)
can you please unpload your entire Project_2 project folder in zip. thus we can test and reproduce the problem ?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Andrew,
can you provide any further information?
What microcontroller are you using? S08 or S12?
How have you these ojbects *defined* (declaration is not enough).
You can use the decoder.exe (or the GNU objdump) utility to inspect your files to see exactly what is in it, see https://mcuoneclipse.com/2012/02/05/show-me-your-files-lib/
I hope this helps,
Erich