No PCIe chapter in datasheet of IMX7Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No PCIe chapter in datasheet of IMX7Dual

458 Views
dwang
Contributor I

Hi FAEs:

There is not a chapter for PCIe in the current version of IMX7Dual datasheet,there is only a chapter for PCIe PHY.

And the PHY supports 6Gbps which is not in PCIe standard.

Why?

Tags (1)
0 Kudos
2 Replies

383 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello D:Wang,

sorry to disgree with you there is a Chapter of the PHY of the PCie in the following Reference Manual:
http://www.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

And let me add that the PCie 2.1  Specification  Supports  6.0Gps since :

PCIe  Allows    2.x (5 GT/s):

  • 500 MB/s (×1)
  • 8 GB/s (×16)


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

383 Views
dwang
Contributor I

For datasheet ,I meant the reference manual.

0 Kudos