How to flash sample programs on MPC5777C EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to flash sample programs on MPC5777C EVB

597 Views
shankarig
Contributor II

How to flash sample programs on MPC5777C EVB? Are there any flash tools available? Any emulators used along with IDE? If yes, any document available to flash the code into target?? 

Labels (1)
0 Kudos
1 Reply

442 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

it depends on the IDE you use.

If you have GHS IDE, you can use Green Hills probe Multi-core JTAG, EJTAG, COP, BDM hardware assisted debugger, embeddeddebugging, on-chip debugging - ... 

If you have S32 Design Studio, you can use Universal Multilink Development Interface Universal Multilink Development Interface|NXP 

Third possibility is to use Lauterbach, which can be used with both IDEs mentioned above and also with some other IDEs and compilers.TRACE32® Qorivva MPC5xxx and SPC5xxx Debugger 

Regards,

Martin

0 Kudos