Hello,
I wonder if an LCD with an 8-bit bus and RGB565 color space is supported in any i.MX product (preferably i.MX6UL).
A pixel is represented by an 16-bit number on the 8-bit bus, so 2 clocks are needed to drive 1 pixel. An example of such LCD is ili9335.
If this is supported:
1) how do I wire this
2) how do I load the driver
I'm using Yocto as operating system and have the DART-6UL demo board.
Thanks!
Jonathan
Solved! Go to Solution.
i80 interface display driver patch is also ready for iMX6UL:
i80 interface display driver patch is also ready for iMX6UL:
Hi Jonathan
seems i80 ili9335 could be supported by i.MX6UL according to
Table 32-3. Pin use in MPU Mode and VSYNC Mode i.MX6UL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
8080 mode driver example
Patch for i.MX28's 8080 mode Lcd panel driver | NXP Community
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------