tools-profile on T4240RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tools-profile on T4240RDB

498 Views
bogdantanasa
Contributor II

We are using linux yocto on a T4240RDB board where we want to have "tools-profile" in our local.conf file. When building the fsl-image-minimal we see that there are some packages that are graphics-related (like gtk+, pixbuf, etc..). The card does not have any graphics capabilities. Why does these packets install at all? Is it possible to have the profiling tools without any gtk dependencies? How the local.conf should look like?

Thanks,

Bogdan.

Labels (1)
Tags (3)
0 Kudos
1 Reply

372 Views
Pavel
NXP Employee
NXP Employee

It looks like that this packages are used in this SDK since there is cross-references in the kernel.

Please keep in mind that Linux is not NXP software.

What you can try is applying all patches from our BSP to the kernel you have, sometimes it works, but generally you should search the community resources for any experience/suggestions on these patches.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos