AnsweredAssumed Answered

About KM34Z256VLL7 AFE pins input range

Question asked by 剑锋 刘 on Aug 22, 2016
Latest reply on Aug 25, 2016 by 剑锋 刘

Hi

I'm using KM34Z256VLL7 in my design, the datasheet describe as follow, and I have some questions to check:

1. Is the full operating voltage range 2.7V~3.3V or -2.7V~3.3V.

2. I know the AFE inputs is 1Vpp differential and 0.5Vpp single ended ,if over the range the ADC result will be saturated, but I can't find the maxium and minimum input range about the AFE pins, if my input voltage is -2V~3.3V,will the AFE module be damaged.

 

Outcomes