settting up ro.sf.hwrotation=9 rotating screen,when only use HDMI output(only one screen)
video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off
08-16 11:31:30.110 508-530/system_process I/DisplayManagerService: Display device added: DisplayDeviceInfo{"Built-in Screen": 1080 x 1920, 60.000004 fps, density 160, 213.0 x 213.0 dpi, touch INTERNAL, rotation 0, type BUILT_IN, FLAG_DEFAULT_DISPLAY, FLAG_ROTATES_WITH_CONTENT, FLAG_SECURE, FLAG_SUPPORTS_PROTECTED_BUFFERS}
Touch screen to work normally
two screen output mode:
video=mxcfb1:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb0:dev=lcd,1024x768,if=RGB24,bpp=32 video=mxcfb2:off video=mxcfb3:off
08-16 11:46:14.030 510-534/system_process I/DisplayManagerService: Display device added: DisplayDeviceInfo{"Built-in Screen": 768 x 1024, 60.000004 fps, density 160, 159.568 x 159.895 dpi, touch INTERNAL, rotation 0, type BUILT_IN, FLAG_DEFAULT_DISPLAY, FLAG_ROTATES_WITH_CONTENT, FLAG_SECURE, FLAG_SUPPORTS_PROTECTED_BUFFERS}
08-16 11:46:14.030 510-534/system_process I/DisplayManagerService: Display device added: DisplayDeviceInfo{"HDMI screen": 1920 x 1080, 60.000004 fps, density 320, 320.0 x 320.0 dpi, touch EXTERNAL, rotation 0, type HDMI, FLAG_SECURE, FLAG_SUPPORTS_PROTECTED_BUFFERS, FLAG_PRESENTATION}
HDMI screen no rotate,so the touch screen resolution ratio is error. I want to know how to solve?
anybody can not help?
Hi Andy
when HDMI screen no rotate, one can try to recalibrate
touch screen so its resolution ratio (boundaries) become normal.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------