AnsweredAssumed Answered

iMX6UL resolution under VGA

Question asked by János Ulbert on Aug 23, 2016
Latest reply on Aug 24, 2016 by János Ulbert

Hi,


I'm find misleading table at the attached pdf file's 25 page.

The table at the right side describes the iMX6UL processor's supported resolutions.
As I see there are no display support under VGA resolution.

 

My intuition is that lower resolutions ! have to OK for the UltraLite, but I have to be sure.

 

I want to use the UltraLite with a 480x272 resolution display is it possible ?

 

Regards János

Outcomes