Hi Everyone:
I am using the i.MX6 Quad serial board with yocto. Then I connect the display with LVDS 1920*1080 to play a 1080p-10M mp4 video.
And the system would randomly crash after 16 ~ 72 hours.
The kernel message only show that
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x08000000
Can any one suggest what happen to that?
Thank you.
Eric
Hi Eric
please try latest nxp L4.1.15 BSP (to exclude OS stability issue) from
also may be useful to run board ddr test
https://community.freescale.com/docs/DOC-105652
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------