If there is any pin on TWR-56F8400-KIT board that is not pointed out have to be connected ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If there is any pin on TWR-56F8400-KIT board that is not pointed out have to be connected ?

676 Views
freemanyang
Contributor II

Hi,

  I am using the demo "BLDC_HS_TWR-56F8400" with TWR-56F8400-KIT, and I did all the steps on Quick Start Guide, the code have aready been download. It seems that all the things are OK, no problem with the BLDCM, but the motor could not work. If anyone have some1similar problems?

  Question is, I heard that I have to connect one of the header to GND or Vcc, which is not mentioned in the documents of thr TWR, I wonder if it is true? Or any one can know what is the problem might be.

Labels (1)
Tags (1)
0 Kudos
1 Reply

431 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Freeman,

I am sorry for the delay.

I suppose that you connect the TWR-8400, TWR_MC_LV3PH board via elevator  board, you need to connect the motor power pins:PHASE_A, PHASE_B,PHASE_C to J5, connect the Hall cable to J6, it is okay.

BR

XiangJun Rong

0 Kudos