AnsweredAssumed Answered

Why my mx28 board with Linux system for mfgtool takes a long time when it is starting

Question asked by jie liu on Aug 21, 2016
Latest reply on Aug 23, 2016 by jie liu

Why my mx28  board with Linux system for mfgtool takes a long time when it is starting : see the attachment in detail

 

first time point

[    3.340000] Trying to unpack rootfs image as initramfs...

[    4.030000] Boot process: fb dev not inited, boot process not start!

[   67.760000] Freeing initrd memory: 6144K

[   68.470000] Bus freq driver module loaded

[   81.600000] mxs_cpu_init: cpufreq init finished

[   89.810000] audit: initializing netlink socket (disabled)

[   89.820000] type=2000 audit(89.820:1): initialized

[  145.100000] JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

second time point:

 

[  167.020000] Console: tianma1 Console: tianma2 Console: tianma3 Console: switching to colour frame buffer device 60x34

[  167.800000] set dclk 8000000 Hz,real lcd clk=8000000 Hz

[ 1039.100000] mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART

[ 1041.890000] mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0

 

third time point

[ 1049.920000] Found APPUART 3.1.0

[ 1058.700000] brd: module loaded

[ 1076.970000] loop: module loaded

[ 1092.350000] Loading iSCSI transport class v2.0-870.

fourth time point : 

[ 1113.490000] Scanning device for bad blocks

 

[ 1137.440000] Boot area protection is enabled.

[ 1137.450000] Creating 2 MTD partitions on "gpmi-nfc-main":

 

Original Attachment has been moved to: output_from_console_with_mfgtool.txt.zip

Outcomes