AnsweredAssumed Answered

Change I2C clock rate on USB-I2C bus interface (OM13518)

Question asked by Kenneth Leung on Aug 18, 2016

I am using the OM13518 to convert serial commands into I2C communication signals to communicate with PCA9536 (4-Bit I/O Port).  Right now the OM13518 is defaulted to 100kHz clock rate which is the slowest rate.  I want to increase the clock rate of the I2C bus interface on the OM13518, but I can't find any programming manual for this product.

Outcomes