Can the i.MX6Solo drive 2 x 1080P30 displays via LVDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the i.MX6Solo drive 2 x 1080P30 displays via LVDS?

570 Views
jamesdavis
Contributor II

Can the i.MX6Solo drive 2 x 1080P30 displays via LVDS?

0 Kudos
3 Replies

484 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

not, as perfomance described in sect.40.4.1 Input Parallel Display Ports

i.MX6SDL Reference Manual (rev.2  5/2015):

for dual input data interface case :

Up to 85 MHz per interface. (WXGA 1366x768 @

60 frames per second, 35% blanking)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

484 Views
jamesdavis
Contributor II

Hi,

Thanks for the response.

However, for external displays, wouldn’t this be an Output LVDS Port?

James

0 Kudos

484 Views
igorpadykov
NXP Employee
NXP Employee

Hi

"dual input data interface" means that

it will be outputed on two separate LVDS Ports.

Best regards

igor

0 Kudos