Dear community,
We have been developing our product with PF3000.
I have a question about Start-up timing diagram.
In Data sheet PF3000 Rev. 7.0, 6.3.3.1 Start-up timing diagram,
it is described that the Start-up timing diagram begins at (VSNVS = 0v) point.
I would like to know the Start-up timing diagram which begins at (VSNVS from LICELL) point.
In the case of MMPF0100, VSNVS starts from 1.0V if LICELL is valid before VIN.
[Question]
Is PF3000 the same behavior as MMPF0100 ?
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
Q. Is PF3000 the same behavior as MMPF0100 ?
A. Yes, the VSNVS output of the PF3000 PMIC behaves the same way as of the PF0100 one.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Artur san,
Thank you for your reply.
I got it.
Best Regards,
Koichi Sakagami
Q. Is PF3000 the same behavior as MMPF0100 ?
A. Yes, the VSNVS output of the PF3000 PMIC behaves the same way as of the PF0100 one.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------