i.MX508: Unused DDR pin termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX508: Unused DDR pin termination

Jump to solution
908 Views
norishinozaki
Contributor V

Hello Champs,

As long as referring to i.MX6 devices, unused DRAM Address, Data,  DQx, CS pins look OK to be float in NC.

Is it true to i.MX50?

BR,

Nori Shinozaki

Labels (1)
0 Kudos
1 Solution
790 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right, if not used these signals can be left float in NC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
791 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right, if not used these signals can be left float in NC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
790 Views
norishinozaki
Contributor V

Hello Igor,
Thanks!

BR,

N.S

0 Kudos