The difference Between PPC64E5500 and PPCE5500 in SDK Download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The difference Between PPC64E5500 and PPCE5500 in SDK Download

690 Views
mohsenhaghighat
Contributor III

hello

when we want to download SDK file for QorIQ processor, there is two file for E5500 processor. what is the difference between these files?

thanks.

Labels (1)
1 Reply

496 Views
Pavel
NXP Employee
NXP Employee

The PPC64E5500 is 64-bit version for the E5500.

The PPCE5500 is 32-bit version for the E5500.

See the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-9D3CDF1C-A65B-4D4C-911C-2...

and

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-E97849FC-67E5-428C-8C37-4...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------