Trying to build standalone applications outside of uboot environment using ./ltib -m shell.
How do I specify the entry point of my application? Can my application start with main()?
If loads command of the u-boot is used for loading .elf file, u-boot reports star address.
See message dump below:
=> loads
## Ready for S-Record download ...
## First Load Addr = 0x00003000
## Last Load Addr = 0x000031E3
## Total Size = 0x000001E4 = 484 Bytes
## Start Addr = 0x00003020
=> go 0x3020
## Starting application at 0x00003020 ...
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------