Can not boot BSC9132QDS from SPIFlash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not boot BSC9132QDS from SPIFlash

1,168 Views
canvanquyen
Contributor III

Hi all,

I have tried several times, to boot bsc9132qds from SPIFlash.

I did as bellow but my images can not boot.

     1. make BSC9132QDS_SPIFLASH_DDRCLK133_config

     2. make

     3. ../boot-format/boot_format ../boot-format/config_ddr3_1gb_9132qds_1330M.dat u-boot.bin -spi bsc9132_SPI133.bin

After that i programmed bsc9132_SPI133.bin to SPI flash, but the board can not boot up event DUT READ LED already ON.

Can anyone help me resolve this problem?

Note : I can boot normally on NAND flash (by make BSC9132QDS_NAND_DDRCLK100_config).

Thanks & Best regards.

Labels (1)
Tags (1)
0 Kudos
3 Replies

821 Views
canvanquyen
Contributor III

Hi all,

Can anyone help me to boot on SPIFLASH for BSC9132QDS?

Thanks & best regards,

0 Kudos

821 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Can Van Quyen,

If you use recent SDK, please try to use config_sram_p1010rdb.dat.

In addition, please check switch configuration to configure your target board in DDRCLK133 and SPI boot mode.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

821 Views
canvanquyen
Contributor III

Thanks Yiping Wang,

I tried it with boot_format : sdk/boot-format.git - Freescale PowerPC SD/SPI boot tool 

And change the boot location to NOR it works well.

anyway, thanks for your answers.

0 Kudos