Hello,
I am confused about I2C baud rate setting.
According to the Table 44-11I2C divider and hold values of datasheet, and the formula: divider = F40 / bit rate = 40MHz / bit rate
I have calculated some baud rate:
1) IBFD.B.IBC = 0x96, divider = 416, then the bit rate should be 40M/416 = 96kHz
but I got the scope like followings, the actual bit rate = 59.3kHz
2) IBFD.B.IBC = 0x20, divider = 160, then the bit rate should be 40M/160 = 250kHz
but I got the scope like followings, the actual bit rate = 102.1kHz
3) IBFD.B.IBC = 0x16, divider = 104, then the bit rate should be 40M/104 = 385kHz
but I got the scope like followings, the actual bit rate = 108.1kHz
And when I use different MCU, the same IBFD.B.IBC value will also cause different bit rate.
So, is the F40 value in the formula (divider = F40 / bit rate = 40MHz / bit rate) different? Then it causes this problem. Where can I find the correct F40 values?
Thanks a lot.
HONG Yang
2016.8.15
Hi,
calculation is correct but the clock is stretched due to weak pull-up. Try to use stronger pull-up resistors on both SCL and SDA lines, for example e.g. 2kOhm.
BR, Petr