Hi
您好!
我不能连接上,你们发给我的链接地址,请你们直接把CAN'的例子程序发给我。我的程序现在就剩下CAN的程序了,没有CAN的程序,不能上车做实验。
If you would like to use FlexCAN component , please first get its license.
! I also attached two example projects for FlexCAN which are not based on PE.
祝好!
At 2016-06-27 16:11:51, "guochunhua" <gch58@163.com> wrote:
Dear sir
I want to encrypt the MCU of 56f84789 in PE of codewarrior 10.4, if 56f84789 is locked and I want to reload program to it, what can I do? how can I encrypt and decrypt 56f84789 in PE of codewarrior 10.4? thank you very much.
Best regards.
guo chunhua
Hello Chunhua
I attached an example project for 56F84789 FlexCAN module, which is based on Processor Expert.
For the project without PE, you can find it in:
https://community.nxp.com/message/651115#comment-651115
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------