AnsweredAssumed Answered

i.MX6SX PMIC Interrupt

Question asked by Balaji Venkatachalam on Aug 11, 2016
Latest reply on Aug 17, 2016 by igorpadykov

Hi all,

    I am planning to use the same PMIC (F6 Version), that is used in i.MX6SX-SDB, in my custom i.MX6SX board.  While reviewing the schematic of the SDB more closely, I observed the PMIC_INT signal is connected to E16 pin of the i.MX6SX. I have the following queries in this regard:

a. Is it configured in the Linux Kernel or is it configured in the U-Boot or is it configured in DTS file, if so which file?

b. Can I use a different GPIO for this purpose (in case if it is configured as a GPIO Input)?

 

Any pointers/references will be much appreciated,

Regards

Balaji.V

Outcomes