Where is the cross compile tool-chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the cross compile tool-chain

Jump to solution
966 Views
dingzhang
Contributor III

I'm using the SABRD board with im6 Quad.

After compiling the Yocto_Project  xwayland: "bitbake fsl-image-qt5"

But where is the cross compile tool-chain??

Thanks a lot

Labels (3)
0 Kudos
1 Solution
700 Views
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
701 Views
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
700 Views
dingzhang
Contributor III

Hi Yuri,

     Thanks for your reply.

     That helps ME a lot. according to your document, i bitbake the tool-chain and succeeded to cross compile my code.

     thanks again

ZHANG DING

0 Kudos