CodeWarrior™ Development Studio for Mac ® OS
CodeWarrior C/C++ Compiler for Mac OS X/PPC.
Copyright (c)2005 Freescale Semiconductor, Inc.
All rights reserved.
Version 4.1 build 448
Runtime Built: Oct 24 2005 12:01:32
Hardware :
Modelnavn: Mac mini
Model-id: PowerMac10,1
Processornavn: PowerPC G4 (1.2) PowerPC 7450
Processorhastighed: 1.25 GHz
Antal CPU'er: 1
L2-buffer (pr. CPU): 512 KB
Hukommelse: 1 GB
Bushastighed: 167 MHz
9.8.0 Darwin Kernel Version 9.8.0: Wed Jul 15 16:57:01 PDT 2009; root:xnu-1228.15.4~1/RELEASE_PPC Power Macintosh
when i type mwcc pq.c -o pq
I get
Warning : Environment varibale 'MWCIncludes' not found
Warning : Environment variable 'MWLibraries' not found
Error : License check fialed: No such feature exists
Feature: MacOS_Plugins_MacOSX_Limited
License path: /Volumes/CW Tools 10.0/Metrowerks CodeWarrior 10.0/
Metrowerks -
CoderWarrior/license.dat
FLEXlm error: -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com"
The second time round having installed the license file, I received by e-mail, something like this came up
mwcc pq.c -o pq
Warning : Environment variable 'MWCIncludes' not found
Warning : Environment variable 'MWLibraries' not found
Error : the file 'stdio.h' cannot be opened
pq.c line 1 #include <stdio.h>
Error : the file 'math.h' cannot be opened
pq.c line 2 #include <math.h>
Checking out diverse discussions, someone mentioned that this would be a licensing problem. How do I solve this and get MWCW to work again?? Your help would be greatly appreciated.
I do not see options, MAC Os versions are not being supported by NXP for several years.