Kernel 4.1.15_1.2.0_ga + i.MX6Q TO1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel 4.1.15_1.2.0_ga + i.MX6Q TO1.0

Jump to solution
1,127 Views
gary_bisson
Senior Contributor III

Hi,

Up until kernel 3.14.52_1.1.1_ga, the TapeOut (TO) 1.0 of the i.MX6Q was supported fine.

But since the 4.1.15_1.2.0_ga, and earlier 4.1.15 tags too, the i.MX6Q TO1.0 doesn't run Linux properly. It seems that the clocking is wrong and the board becomes very slow.

The Release Notes doesn't mention any minimal processor revision so it is assumed even the TO1.0 should be supported.

Please advise.

Regards,

Gary

Labels (2)
0 Kudos
1 Solution
627 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gary

it was dropped since L3.0.35_4.1.1

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gary

it was dropped since L3.0.35_4.1.1

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
627 Views
gary_bisson
Senior Contributor III

Hi Igor,

Thanks for your answer. I wish this line was still on current Release Notes, we have customers using TO1.0 that don't understand why 4.1.15 isn't working.

Regards,

Gary

0 Kudos