PF3000 : VCC_SD voltage transition time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 : VCC_SD voltage transition time

Jump to solution
596 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with PF3000.
I have a question about  VCC_SD voltage transition time.

The VCC_SD voltage is switched by SD_VSEL logic level.

[Question]
       How long time does it take to switch the VCC_SD voltage range by changing SD_VSEL ?

    Best Regards,
    Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
507 Views
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

unfortunately this time is not specified by datasheet, however one

can estimate it using formula : I*t=C*U,

I=100mA, U=3V (SD_VSEL, Vh-Vl),C=2.2uF,

t~60uS

Best regards

igor
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
508 Views
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

unfortunately this time is not specified by datasheet, however one

can estimate it using formula : I*t=C*U,

I=100mA, U=3V (SD_VSEL, Vh-Vl),C=2.2uF,

t~60uS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos