I get various valgrind build errors when I do a bitbake fsl-image-full. Are there patches for these?
We usually use the following command sequence for SDK installing under Ubuntu 14.04 and Ubuntu 16.04:
1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos
2. a) command: ls -l /bin/sh
Message: /bin/sh -> dash
b) command: sudo dpkg-reconfigure dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
c) command for checking: ls -l /bin/sh
Message: /bin/sh -> bash
3. install SDK cache for e6500
4. install SDK source
5. cd <sdk-install-dir>.
6. ./sources/meta-freescale/scripts/host-prepare.sh
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
Look at your Linux message dump. Are there error messages at "./sources/meta-freescale/scripts/host-prepare.sh" command?
7. bitbake fsl-image-minimal
8. bitbake fsl-image-full
Look at the following page about valgrind using:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
79808949