In my design,DDRCLK = 133.3MHz.
I want to set that DDR Bus CLK = 667MHz,DDR data rate = 1333MHz.
So I should choose MEM_PLL_RAT = 00_0101?
But when I config rcw through QCVS,I select DDR data rate/DDRCLK = 10:1,
then DDR data rate is displayed as 1.33GT/s,
the MEM_PLL_RAT = 00_1010.
Which one is correct?
Thanks.
> So I should choose MEM_PLL_RAT = 00_0101?
No.
Please note that above the shown table it is written:
"This field selects the DDR data rate to DDRCLK ratio"
The DDR data rate is two times higher than DDR bus clock.