Maximum rating about LICELL of MMPF0100NPAZES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum rating about LICELL of MMPF0100NPAZES

451 Views
inhojeon
Contributor III

Hi, All.

Below circuit is designed refer to SABRE Bd of i.MX6DL.

pastedImage_0.png

I wonder about 'Maximum level' of 'LICELL' about 'MMPF0100NPAZES.'

Because charging voltage of 'LIR2450(Li-on Battery)'is '4.2V.'

So, I'll set output level of 'U4(LT3012HFE#PBF)' is '4.2V.'

But see the datasheet of  'MMPF0100NPAZES', max. level of 'LICELL' is 3.6V like below.

pastedImage_3.png

I think ordinary li-on battery of charging level is '4.2V.'

So,I want to know that it is possible to use '4.2V' level for 'LICELL' of 'MMPF0100NPAZES'.

Please, Inform me about that questions, ASAP.

Best Regards,

Inho Jeon

Labels (2)
Tags (1)
0 Kudos
1 Reply

379 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The MMPF0100  Datasheet is correct : maximum allowed LICELL voltage is 3.6 V.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos