AnsweredAssumed Answered

Controlling RGB Led from imx6sl connected to pwm pin

Question asked by sandeep sharma on Aug 3, 2016
Latest reply on Aug 5, 2016 by sandeep sharma

Hi Team

 

I am working on Free-scale imx6sl and I have to control NeoPixel Digital RGB led which will be connected to it over pwm.

From documents i can see that there are 4 pwm pins in imx6sl.

PWM-1

PWM-2

PWM-3

PWM-4

 

Can someone please suggest how can i proceed here.Is there any existent driver for it ?

 

RGB Led Details:-

  • Maximum 5V @ 60mA draw per 1.3" strip segment (all LEDs on full brightness)
  • 5VDC power requirement (do not exceed 6VDC) - no polarity protection
  • The frequency of PWM FPWM --- 1.2 --- KHZ ---

 

Regards

Sandeep S

Outcomes