Hi,
I am new to kernel programming. I would like to redirect the kernel dmesg output via the UART2 of T4240RDB.
What is the procedure for the same?
I found the links which which describes the generic process Electronics FAQ: Redirecting kernel messages (dmesg) out through your serial port
But on T4240RDB ttyS0 (UART1) is used for the console to access the linux from the host.
Now , I want the dmesg output to be redirected to the ttyS1 (UART2) of T4240RDB.
Is it possible . What are the steps to achieve it. Should I add a boot parameter in the u-boot?
A quick response is appreciated as I am stuck with an issue here.
Thanks in advance.
Sareena.