AnsweredAssumed Answered

SDK 2.0 on P5020

Question asked by Darren Stevens on Jul 30, 2016
Latest reply on Aug 9, 2016 by Yiping Wang

I'm trying to build a kernel for our custom P5020 board with linux SDKv2.0, but my kernel doesn't work.

 

Our board can be supported by adding an additional match string to corenet-generic.c, and my build system works, as I have tested it by building a 4.1.28 from kernel.org, which works perfectly.

 

When I attempt to run my SDK kernel the output stops right after the U-Boot line:

   'Loading Device Tree to 03f5000, end 031fff57' - no more output on console or serial. The machine has just hung.

 

I did notice a couple of messages that don't occur with the kernel.org build:

make: Circular arch/powerpc/lib/crtsavres.o <- prepare dependency dropped.

make[1]: 'arch/powerpc/lib/crtsavres.o' is up to date.

 

What do I need to do to get this to build properly?

Thanks.

Darren

Outcomes