hi
i have builded a yocto project,and used the
Yocto Project 2.0 | Jethro |
the local.conf:
MACHINE ??= 'imx6ulevk'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"
DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"
BB_NUMBER_THREADS = '8'
PARALLEL_MAKE = '-j 8'
after bitbake core-image-sato.(done)
i got the files :
i want to using the mfgtool on pc ,no u-boot.imx.
so i done this:
bitbake -c clean u-boot-imx (done)
bitbake -c patch u-boot-imx (done)
bitbake -c compile -f u-boot-imx (error)
log:
| ./tools/mkimage -n board/freescale/mx6ul_14x14_evk/imximage.cfg.cfgtmp -T imximage -e 0x87800000 -d u-boot.bin u-boot.imx
| Image Type: Freescale IMX Boot Image
| Image Ver: 2 (i.MX53/6 compatible)
| Mode: DCD
| Data Size: 360448 Bytes = 352.00 kB = 0.34 MB
| Load Address: 877ff420
| Entry Point: 87800000
| make[1]: Leaving directory `/home/lyi/imx/fsl-connunity-bsp-jethro/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git/mx6ul_14x14_evk_config'
| cp: cannot stat '/home/lyi/imx/fsl-connunity-bsp-jethro/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git/mx6ul_14x14_evk_config/u-boot.img': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/lyi/imx/fsl-connunity-bsp-jethro/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/temp/log.do_compile.31796)
ERROR: Task 4 (/home/lyi/imx/fsl-connunity-bsp-jethro/sources/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2015.04.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 240 tasks of which 238 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/lyi/imx/fsl-connunity-bsp-jethro/sources/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2015.04.bb, do_compile
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
lyi@imx:~/imx/fsl-connunity-bsp-jethro/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git/mx6ul_14x14_evk_config$ ls
arch common drivers fs lib net source test u-boot u-boot.imx u-boot.map
board disk examples include Makefile scripts System.map tools u-boot.bin u-boot.lds u-boot.srec
i have tried this:
bitbake -c clean u-boot (done)
bitbake -c patch u-boot (done)
bitbake -c compile -f u-boot (error)
there was no error , no u-boot.imx.
u-boot-fslc was the same phenomenon。
only the u-boot-imx i can got u-boot.imx
but what's the mean of the error,why?
Q1:
how can i got the u-boot.imx?
Q2:
the different about these(u-boot ,u-boot-imx, u-boot-fslc)?
thanks for you help!
Hi
u-boot.imx can be found
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_4.1.15_1.0.0_ga
regarding differencies please check attached Yocto Guide
sect.5.5 U-Boot configuration, sect.3.1 Host packages and link
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi
thanks for you help!
my bsp is L3.14.52.
it's the same reason?
how can i build the u-boot.imx by bitbake?
thanks!