Hi
Ours is a custom board based on imx6 we are currently using Android Kitkat 4.4.3.The Kernel consist of Android Linux 3.10.53 and root file system consist of kitkat.But as soon as the systems is booted i get a android logo after which the screen becomes blank. when i give logcat to see the android level log.we have noticed a log stating
W/SurfaceFlinger( 109): Timed out waiting for hw vsync; faking it
is this the reason the android GUI is not coming up or is there any other change need to be done in file system.
Please let me know and thanks in advance.
Thank you,
Deepanraj.A
Hi Deepanraj
please try
Android 4.4.3 Kitkat Patch (KK4.4.3_2.0.1) and KK4.4.3 source code on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------