I have a test project I'm trying to build using two JN5168 radios, with the JPT running on both.
However I'm having an odd issue where once a radio sends anything, it can no longer receive until it's reset.
I looked over the JN-AN-1172 code and I'm doing essentially the same thing as it does: when I want to transmit I use "vJPT_PacketTx" with the channel and the packet structure, and when I am trying to read the data I use "bJPT_PacketRx".
Is there anything I can do about this?
I found the answer to the issue: there is a bug in the JPT driver causing this issue.
However, changing channels resolves the issue. So I just have it change the channel and then change back.