Dear community,
I followed the steps described in the Quick Start Guide:
* Download Software from freescale.com\sensortoolbox
* Installed Software - no Errors occured
* Connected Evalboard to USB-port and switched the power Switch to on (red led is on)
* FTDI-Driver is installed (checked in Device Manager)
* Software started
and then it appears a window "Loading Freedom Sensor Toolbox(CE) - Please wait..." and nothing happens
Can anybody help?
Thanks
Frank
Solved! Go to Solution.
Dear Frank,
Could you please specify which development board are you using? If it is the RD4247MAG3110 (LFSTBEB3110), please download and install the E-Compass Sensor Toolbox v6.1.0.1.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
I can not download the E-Compass Sensor Toolbox v6.1.0.1, it say Page Not Found
can you sent it to my email 364023214@qq.com .thanks very much. i really need it now. I'm looking forward to your reply.
Dear Frank,
Could you please specify which development board are you using? If it is the RD4247MAG3110 (LFSTBEB3110), please download and install the E-Compass Sensor Toolbox v6.1.0.1.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Dear Tomas,
yes, indeed it is the LFSTBEB3110 Magnetometer Development Board. With your help and downloading the E-Compass Sensor Toolbox it works now.
Maybe it is worth thinking about adding this Detail to the Quick Start Guide.
Nevertheless Thanx for your quick Response.
Regards
Frank