MPC5674F PLL Jitter on D_CLKOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F PLL Jitter on D_CLKOUT

Jump to solution
899 Views
JDFAE
NXP Employee
NXP Employee

A have a customer who is using an MPC5674F at 264MHz. They drive EXTAL with a 12MHz hybrid oscillator so the input source is stable.

 

On the D_CLKOUT pin, they are seeing more than a little jitter coming out of the PLL. They haven’t spent time trying to understand the ins and outs of jitter measurements to quantify exactly how much jitter there is.  There’s nothing visible for jitter on the 12MHz clock input, perhaps 1-2 percent on the D_CLKOUT pin.

 

They are concerned since the D_CLKOUT becomes the reference clock for a PLL in an external FPGA most likely exacerbating that PLL’s jitter.

 

They’re going back into layout soon and would like a recommendation of what can be done to minimize the 5674 PLL’s jitter. They have an LC filter on the VDDSYN input and are planning to get the components as close as possible to
the pin.

Labels (1)
1 Solution
809 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

max jitter is specified as +/-5% of CLKOUT frequency, so 1-2% is still within limit.

pastedImage_0.png

pastedImage_1.png

Yes, to keep the jitter as low as possible, it is necessary to use stable external clock, filter supply voltage enough (especially VDDSYN) and follow general PCB design rules...

Regards,

Lukas

View solution in original post

1 Reply
810 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

max jitter is specified as +/-5% of CLKOUT frequency, so 1-2% is still within limit.

pastedImage_0.png

pastedImage_1.png

Yes, to keep the jitter as low as possible, it is necessary to use stable external clock, filter supply voltage enough (especially VDDSYN) and follow general PCB design rules...

Regards,

Lukas