Hi,
I'm trying to use an I2C gyroscope (L3G4200D) on Karo TX6DL (iMX6DL), I think that the bit start is generated because the IBB bit toggle from 0 to 1, but I don't receive an acknowledge from the slave, when I control scl pin with oscilloscope, I don't find a clock signal.
Where is the problem ?
Hi Djillali
it may be recommended to check if SION bit is set in i2c
iomux registers IOMUXC_SW_MUX_CTL_PAD_KEY_X.
Also please check if clock is enabled in CCM_CCGR register.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------