Hello,
when debugging with the Kinetis K22F i used openOCD. When I go there with my mouse pointer over the variable view, the content of the variables is displayed.
Now I needed to switch to JLInk as I want to use my custom board, and if I hover now over the variables in the debug view - no variable content is displayed.
How Do I get that the variable contents are displayed using KDS 3.2 and Segger JLink?
-Michael
Hello Michael,
In KDS , you can use the "Expressions view" to view variable :
you can open this view at the Window :
And also when you put the mouse point over the variable ,it also can show the data 。
Hope it helps
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------