Our main requirement was to playback any mp4 video from MMC at a resolution of 1024x768 @50 Hz on i.MX6-SOLO .
We tried to play the MP4 video with different resolutions.
When we played MP4 video with 720 x 480 resolution of 2 min length, the occupied memory is getting free from RAM.
So, we thought playing high resolution video is the issue, as we are playing 1280*720 resolution of 1.01 hour length video .
But when we played MP4 videos with different resolution of 1 hour length, we faced the same issue, but now the memory consumption is slow for less resolution videos.
Please find the attachment, we checked the memory consumption with free command.
$gplay Demo.MP4
is the command which we are giving to play the video
Original Attachment has been moved to: subra_gplay_2.08min.txt.zip
I'm not sure what bsp version you use, the below link discuss the mx6 memory leak issue, one can refer to it.