How to change Internal oscillator frequency to 24MHZ on LPC11C14?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change Internal oscillator frequency to 24MHZ on LPC11C14?

622 Views
kalpeshbalar
Contributor II

How to change Internal oscillator frequency to 24MHZ on LCP 11C14?

I wan to achieve maximum possible speed on LPC11C14. Need is to update LCD with Maximum rate.

I am using LPC open libraries on LPC expresso.

Please suggest changes for above requirement.

 

Also I have tried to connect 24MHz Crystal but with this crystal firmware is not working. If I connect 12MHz crystal it is working fine.

 

How to calculate time taken by one Machine cycle on LPC11C14?

 

Thanks,

KBalar

Labels (1)
Tags (2)
0 Kudos
1 Reply

472 Views
magicoe_niu
NXP Employee
NXP Employee

Hi,

Internal IRC is 12Mhz, you may use PLL to generate 24Mhz from 12Mhz.

Thank you!

Thank you!
0 Kudos