AnsweredAssumed Answered

S32DS Project with MAC57D5xx, A5 project not able to start

Question asked by nitin dhingra on Jul 24, 2016
Latest reply on Aug 1, 2016 by stanish

Hi,

I have a MAC57D54H board with PE Micro debugger connected to it.

I Create a new S32DS Project choosing Family MAC57D5xx with all the toolchain selected, M4, A5 and M0+.

Three projects are created and I select and build the A5 project; then click on debug (choosing Debug Debug_RAM or release, any of the options).

Debug progress gets stuck at 90% (message says "configuring GDB") and after waiting for sometime I get a message

"Launching NXM_XXXXX_A5_Debug_RAM has encountered a problem" and in the details Section it is written as follows:

 

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:7226

Error message from debugger back end:

localhost:7226: The system tried to join a drive to a directory on a joined drive.

localhost:7226: The system tried to join a drive to a directory on a joined drive.

 

 

I created this project with default settings and have PE Micro as the debugger connected to the PC and the board.

 

Whereas If I choose M4 project it debugs and runs without any error.

 

Any Idea what is the issue or how I can make A5 run on this board with default project?

My main intention is to run both A5 and M4 on the board.

 

regards

nitin

Outcomes