Aaron Lager

coldfire lite tcp/ip 2.0 UART doesn't work

Discussion created by Aaron Lager on Jun 11, 2008
Latest reply on Jun 12, 2008 by Aaron Lager
Once I compiled the web server target for the 52235evb the UARTs stop working.
I'm using the 2.0 version of the internich software from this link:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=COLDFIRE_TCPIP&fsrch=1

The UARTs worked before I put this code onto the board, giving the terminal outputs.
Any ideas on what to check?

From processor.h:
Code:
#define CONSOLE_UART 0  /* Set to the respective UART number to use for console *//* Default is 0; 1 works if evb supports it; 2 and above not configured in software/hardware  */#define FULL   0#define HALF   1#define DUPLEX   HALF //FSL enter HALF or FULL to select Ethernet duplex mode

I just ran across this:
Code:
#ifdef USE_COMPORT
but I can not find it defined anywhere (using find all).  Where should this be defined?

Thanks,
Aaron
 

 


Outcomes