AnsweredAssumed Answered

Freemaster with FRDM-KE06Z

Question asked by Bruno Tremblay on Jul 20, 2016
Latest reply on Oct 8, 2018 by Marcio L. Carleto

Hello,

 

I was able to connect Freemaster to a FRDM-KL25Z following the instructions on MCU on Eclipse: Tutorial: FreeMASTER visualisation and run-time debugging. The visualization works fine. Now I try to connect to a FRDM-KE06Z without luck. I alwas get the "Can not get board information! The communication will be pause. Error code 0x80000101"

 

I try with an up date of the OpenSDA (1.18). I notice that the FreeMaster's Processor Expert bean with the KE06 is different from the one with the KL25, but not much.

 

Did someone have success using FreeMASTER on a FRDM-KE06Z?

 

Best Regards,

Bruno

Outcomes