The document below has the following:
RT-tests suit contains various test applications like cyclictest, hackbench, etc to measure latencies and induce various test loads.
https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-5E34A886-778F-470E-8C9B-5...
How do we build the RT-tests as a package in yocto and build it into the rootfs? We do not see a package for the RT patch supported for local.conf when building. What enables the Yocto RT-test package in yocto?
Also, can it be built for both the core and full image builds?
Also it should be noted, PREEMPT_RT has been validated on the LS1043ARDB by NXP.
The name of the SDK package that contains rt tests is 'rt-tests'
The article at the URL below describes how to add packages to the rootfs:
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------